Smarter
Mobility

The future of mobility is smarter – it promises clean, sustainable and low-noise mobility solutions.Leading the way in this field, ABB is taking an important step towards an emission-free future: Smart fast-charging systems at petrol stations, motorway ser vice stations or at home ensure that the dream of electric cars, buses, trucks, boats, and even racing cars, will come true.

 

Charging infrastructure

Charging is the new refuelling. Fast, easy and available everywhere. Right there where you are. With electromobility, you maintain the flexibility you’ve come to expect.

infographic-mobility

Charging systems
for every application

DC fast-charging systems

With more than 6,000 networked charging stations in over 50 countries, ABB is today the global market leader in fast-charging solutions for electric cars. The charging stations can be easily connected to any service or payment application and the firmware of the stations is updated regularly.

Terra 53 series

The Terra 53 DC charging station is suitable for motorway service stations, petrol stations, car dealerships, branches and heavily frequented inner-city areas.

  • Charging time 15–30 minutes,
    depending on the size and current
    cap­acity of the battery

EVLunic – AC Wallbox

The wall charging stations which con­veniently charge your electric car at home, operate with alternating current. AC variants from 4.6 kW to 22 kW are available, depending on the application. Charging time is four to eight hours, depending on the size and current capacity of the battery.

  • Compatible with all common
    electric and hybrid vehicles
  • Minimal space requirements
    and costs

Flexible and
independent

Charge overnight and
climb into a fully charged
electric car in the morning.

Formel E

Two pioneers
writing the future
of mobility

As the main sponsor of the ABB FIA Formula E Championship racing series, ABB is putting its expertise in the field of electricity grids, electric mobility and fast-charging solutions at the disposal of electric motor sport. The FIA Formula E Championship is the worldʼs first motor sport series thatʼs dedicated exclusively to electric racing cars. However, it is much more than just a racing series: Formula E offers a unique opportunity to develop and test sustainable technologies for power generation and transmission as well as electric mobility for everyday use. Together with Formula E, ABB is  shaping the future of electric mobility, not only in motor sport but also in everyday life.

abb-formula-e

Formula E and ABB bring excitement to the worldʼs roads. All dates, all races – hereʼs the 2018 season at a glance.

Mar

formel-e-line1-9x363-abb

Punta Del Este
17|03

Apr

formel-e-line2-9x201-abb

Rome
14|04

Apr

formel-e-line1-9x363-abb

Paris
28|04

May

formel-e-line2-9x201-abb

Berlin
19|05

June

formel-e-line1-9x363-abb

Zurich
10|06

July

formel-e-line2-9x201-abb

New York
14–15|07